Vishay Intertechnology Releases New Power Metal Strip« Resistor in Compact 0612 Case Size

Featuring Wide Side Terminal Construction, Device Offers High 1 W Power Rating and Low Resistance Down to 0.001 Ω


WSL0612

Products mentioned:

WSL, Wide Terminal
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
MALVERN, Pa. — June 3, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today launched a surface-mount Power Metal Strip« resistor with a wide side terminal construction that yields a high 1 W power rating in the compact 0612 case size. The new WSL0612 combines its high power-to-footprint-size ratio with extremely low resistance values down to 0.001 Ω and stable resistance tolerances to 1.0 %.

The advanced construction of the WSL0612 resistor incorporates a solid metal nickel-chrome alloy resistive element with low TCR (< 20 PPM/░C). This results in a high-power resistor in the 0612 package size that maintains the superior electrical characteristics of the Power Metal Strip construction. The device’s small size allows for the design of high-power circuits featuring the smallest possible resistor for higher-performance end products.

The resistor is ideal for all types of current sensing and pulse applications, including switching and linear power supplies, instruments, power amplifiers, and shunts in automotive electronic controls such as engines, brushless DC motors, anti-lock brakes, climate, and battery management controls; industrial controls, including down-hole test/measurement equipment for oil/gas well drilling; inverter controls for HVAC systems; and DC/DC converters for servers, VRMs for laptops, and Li-Ion battery safety and management.

Like all Power Metal Strip resistors, the device released today features an all-welded construction that contributes to its superior electrical performance. A proprietary processing technique produces extremely low resistance values ranging from 0.001 Ω to 0.003 Ω, with tight tolerances of 1.0 %, and 5.0 %. The WSL0612 provides low thermal EMF (< 3 ÁV/░C) and a temperature range from -65 ░C to +170 ░C. The device is lead (Pb)-free, RoHS-compliant, and Vishay Green.

Samples and production quantities of the new resistor are available now, with a lead time of five to seven weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology