New Vishay Intertechnology Power Metal Strip« Resistor Offers Eight Times the Power Dissipation of Other Devices in Compact 0805 Package Size

Space-Saving Current Sense Resistor Delivers High 1 W Power Rating for Automotive and Computer Applications


WSLP0805...18

Products mentioned:

WSLP...18
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
MALVERN, Pa. — June 30, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new surface-mount Power Metal Strip« resistor featuring a high 1 W power rating in the compact 0805 package size. Designed to save space in automotive and computer applications, the Vishay Dale WSLP0805...18 combines its high power-to-footprint-size ratio with extremely low resistance values down to 0.005 Ω.

The advanced construction of the WSLP0805...18 resistor incorporates a solid metal nickel-chrome or manganese-copper alloy resistive element with low TCR (< 20 PPM/░C). This results in a high-power resistor in the 0805 package size that maintains the superior electrical characteristics of the Power Metal Strip construction. The device’s small size allows it to replace larger current sensing resistors, saving space on the circuit board that in turn will create smaller and lighter products for the consumer.

Offering eight times the power dissipation of other devices in the 0805 package size, the WSLP0805...18 is ideal for all types of current sensing and pulse applications, including switching and linear power supplies, instruments, power amplifiers, and shunts in automotive electronic controls such as engine, transmission, audio electronics, and climate controls; and DC/DC converters for servers, VRMs for notebook computers, and Li-Ion battery safety and management. For increased reliability, a reduced CTE (coefficient of thermal expansion) mismatch with the PCB reduces the possibility of solder joint cracks resulting from thermal cycles.

Like all Power Metal Strip resistors, the device released today features an all-welded construction that contributes to its superior electrical performance. A proprietary processing technique produces extremely low resistance values ranging from 0.005 Ω to 0.01 Ω, with tight tolerances down to ▒ 1.0 %. The WSLP0805...18 provides very low inductance of 0.5 ηH to 5 ηH, an excellent response to 50 MHz, low thermal EMF (< 3 ÁV/░C), and a temperature range from -65 ░C to +170 ░C. The lead (Pb)-free device is RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the new resistor are available now, with lead times of six to eight weeks for larger orders.

Resources:

Power Metal Strip resistors

Check distributor stock on the Vishay website

Weekly updates: sign up for Vishay Newsfeed

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology