Vishay Interchnology Enhances T55 Series of Polymer Tantalum Chip Capacitors With Higher Capacitance to 470 F and Lower ESR to 25 mΩ in A, B, and T Case Sizes


T55

Products mentioned:

T55
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
MALVERN, Pa. — July 1, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has enhanced its T55 series of vPolyTan surface-mount polymer tantalum molded chip capacitors with eight new ratings in the A, B, and T (low-profile B − 1.2 mm max.) case sizes. Taking advantage of Vishay's market-leading package technology and recent investments in polymer tantalum technology, the Vishay Polytech T55 series now offers significantly higher capacitance and lower ESR for computer, telecom, and industrial applications.

At 2.5 V, capacitors in the B case now offer higher capacitance to 470 F with ESR of 25 mΩ, in addition to lower ESR of 25 mΩ at a capacitance of 330 F. At 6.3 V, devices in the A and T case sizes provide improved ESR of 70 mΩ at 100 F, while B case devices feature lower ESR of 40 mΩ at 33 F and 35 mΩ at 220 F. At 10 V, devices in the B case size offer enhanced ESR of 70 mΩ at 47 F.

The low ESR of the T55 capacitors is a result of their polymer cathodes, which offer greatly enhanced performance over manganese dioxide devices. In addition, the devices offer excellent ripple current rating up to 2.28 A IRMS and provide low internal resistance for enhanced charge and discharge characteristics. The capacitors are optimized for power management, battery decoupling, and energy storage in computers, tablets, smart phones, wireless cards, and solid state drives.

Offered in the compact J, P, A, B, and T case sizes, the T55 series features a wide capacitance range from 3.3 F to 470 F over voltage ratings from 2.5 V to 10 V, and a capacitance tolerance of 20 %. The devices provide ultra-low ESR from 500 mΩ down to 25 mΩ at +25 C and 100 kHz, and operate over a temperature range of -55 C to +105 C with voltage derating above +85 C.

Featuring lead (Pb)-free terminations, T55 series capacitors are RoHS-compliant, halogen-free, and Vishay Green. The devices are compatible with high-volume automatic pick-and-place equipment and offer a Moisture Sensitivity Level (MSL) of 3.

Samples and production quantities of the enhanced T55 series are available now, with lead times of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

vPolyTan is a trademark of Vishay Intertechnology