Vishay Intertechnology’s UMB 0207 MELF Resistor Receives EDN China 2015 Innovation Award in Passive Components Category


UMB 0207

Products mentioned:

UMA 0204, UMB 0207
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
MALVERN, Pa. — July 17, 2015 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its UMB 0207 series of ultra-precision thin film MELF resistors has won an EDN China 2015 Innovation Award. The UMB 0207 received a Leading Product Award in the Passive Components category at an award ceremony on June 25 in Shanghai. Senior sales manager Dennis Tang was on hand to receive the award on behalf of Vishay.

The EDN China Innovation Awards were introduced in 2005 to recognize achievements in the design of ICs and related products in the Chinese market. They have steadily grown to become one of the China Mainland’s most anticipated and respected accolades for the electronics design industry. This year, 161 products from 102 companies entered the Product Awards in 14 categories. Finalists were shortlisted by EDN China analysts, and winners were selected through online voting, expert judging, and analyst evaluation.

“I am honored to receive this award on behalf of Vishay,” said Dennis Tang, senior sales manager, Vishay. “The EDN China Innovation Awards are very prestigious awards, and we are proud to be selected to receive one this year for the UMB 0207 series of ultra-precision thin film MELF resistors.”

Vishay’s UMB 0207 series combines the proven reliability of professional MELF products with the most advanced level of precision and stability ever achieved with axial thin film high-precision resistors. This unique combination makes the devices perfectly suited for precision circuits in measurement and calibration equipment, industrial process control systems, aerospace electronics, and medical equipment.

Offered in the standard 0207 case size, the UMB 0207 features a temperature coefficient of resistance (TCR) down to 5 ppm/K, a resistance range from 100 Ω to 390 kΩ with tolerances down to 0.02 %, high operating voltage of 350 V, rated power dissipation to 400 mW at +70 C, and excellent long-term stability down to < 0.02 % after 1,000 hours. Suitable for processing on automatic SMD assembly systems, the devices are completely Green — lead (Pb)-free, halogen-free, and RoHS-compliant without exemptions.

For more Chinese-language information on the EDN China 2015 Innovation Awards, please visit http://www.ednchina.com/award/2015/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.