MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology Releases Commercial Version of the Popular Automotive Grade IHLE Integrated E-Shield Inductor

Available in 2525, 3232, and 4040 Case Sizes, Devices Provide -20 dB Electric Field Reduction at 1 cm


For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Jan. 16, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a commercial version of its popular Automotive Grade IHLE series of low-profile, high current inductors featuring integrated e-shields for EMI reduction. Available in the 2525, 3232, and 4040 case sizes, the Vishay Dale IHLE-2525CD-51, IHLE-3232DD-51, and IHLE-4040DD-51 contain the electric field associated with EMI in a tin-plated copper integrated shield, providing up to -20 dB of electric field reduction at 1 cm (above the center of the inductor) when the integrated shield is connected to ground. By eliminating the need for expensive board-level Faraday shielding to lower EMI, the devices reduce costs and save board space.

Featuring high temperature operation to +155 ░C and coplanarity of their four terminals within ≤ 100 Ám, the inductors released today are optimized for energy storage in DC/DC converters and high current filtering. Applications include notebooks, desktop PCs, and servers; high current point-of-load converters; graphics cards; DC/DC converters for distributed power systems and FPGAs; and telecom infrastructure.

Built on Vishay Dale IHLP« technology, the IHLE-2525CD-51, IHLE-3232DD-51, and IHLE-4040DD-51 feature high efficiency with typical DCR from 1.55 mΩ to 167 mΩ and a wide range of inductance values from 0.22 ÁH to 47 ÁH. The devices provide rated currents to 36.0 A and handle high transient current spikes without saturation.

Packaged in an RoHS-compliant, 100 % lead (Pb)-free shielded construction, the inductors offer high resistance to thermal shock, moisture, and mechanical shock. In addition, devices’ 4-terminal connection (two ground connection points for the shield) provides high vibration performance for on-engine and chassis-mounted electronic circuits. The devices are halogen-free and Vishay Green.

Device Specification Table

Part number IHLE-2525CD-51 IHLE-3232DD-51 IHLE-4040DD-51
Inductance @ 100 kHz (ÁH) 0.47 to 22 0.22 to 33 0.47 to 47
DCR typ. @ 25 ░C m(Ω) 3.87 to 163.0 1.68 to 149.0 1.55 to 167
Heat rating current typ. (A) 2.8 to 22.0 3.1 to 36.0 2.5 to 30.0
Saturation current typ. (A) 2.2 to 14.0 3.2 to 32.0 4.5 to 28.5

Samples and production quantities of the new IHLE devices are available now, with lead times of 10 to 12 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

IHLP is a registered trademark of Vishay Intertechnology

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH