MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology Automotive Grade Power Metal Strip® Battery Shunt Resistor Offers Improved Accuracy, Corrosion Protection

36 W Device Features Low Resistance Down to 50 µΩ, Tin Plating to Aid in PCB Mounting


WSBS

Products mentioned:

WSBS8518...14
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — March 27, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new Automotive Grade Power Metal Strip® battery shunt resistor that offers a 36 W power capacity in the 8518 case size with tin plating on the terminals. Featuring extremely low resistance values down to 50 µΩ, the Vishay Dale WSBS8518...14 will lead to increased accuracy and lower costs compared to Hall Effect current sensing solutions, while its tin plating assists with PCB mounting and provides increased protection against corrosion.

The AEC-Q200 qualified device released today features a proprietary processing technique that produces extremely low resistance values of 50 µΩ, 100 µΩ, 125 µΩ, and 250 µΩ. These low values will allow for more accurate data to determine battery charge and discharge, thus helping designers meet specific customer battery management requirements for applications in gas, diesel, hybrid, and electric cars and trucks, as well as electric forklifts and other heavy industrial applications.

The WSBS8518...14 features a solid metal manganese-copper alloy resistive element with low TCR (± 20 ppm/°C), and an all-welded construction. The resistor offers low inductance values of < 5 nH, low thermal EMF down to < 1 µV/°C, and an operating temperature range of -65 °C to +170 °C. The device is RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the WSBS8518...14 are available now, with a lead time of 8 to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH