MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology PR02-FS High Pulse, Fusible, Non-Inductive, Flameproof Metal Film Resistor Offers Defined Fusing Characteristics

Device Meets the Safety Requirements of UL1412, Features Resistance > 50 Ω to Handle 600 V Surges


PR02FS

Products mentioned:

PR02-FS
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — April 3, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new high pulse, non-inductive, fusible, flameproof metal film resistor that meets the safety requirements of UL1412. The Vishay BCcomponents PR02-FS offers defined fusing characteristics at defined overload conditions, and resistance values > 50 Ω to withstand 600 V surges (1.2/50 s pulse) as defined by IEC 61000-4-5.

With its defined fusing behavior and fast fusing time of < 10 s for an 80 W overload, the device released today is designed to disconnect electronic home appliances such as washing machines and shaver chargers from the power supply. In addition, it provides current limiting in low voltage power supplies for indoor lighting applications. Moreover, due to its inherent non-inductive design, it can be used in applications such as snubber circuits with inductive loads.

The PR02-FS offers a resistance range from 1 Ω to 100 Ω with tolerance down to 10 %, TCR of 250 ppm/K, rated power dissipation of 2 W at +70 C, and an operating temperature range from -55 C to +200 C. Available in a radial version, the device meets active and passive flammability requirements as defined by IEC 60115-1 and UL 94-V0. The resistor is RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the PR02-FS are available now, with lead times of 8 to 10 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in: