MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

New Vishay Intertechnology AEC-Q200 Qualified Inductor Is Industry’s First With 125 A Continuous Current Rating

Device Features 190 A Saturation Current for 20 % Inductance Reduction and Continuous High Temperature Operation to +155 C


IHXL

Products mentioned:

IHXL-2000VZ-5A
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — April 26, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new AEC-Q200 qualified inductor that is the industry’s first to offer a continuous current rating of 125 A. For automotive and industrial applications, the Vishay Dale IHXL-2000VZ-5A features a 190 A saturation current for 20 % inductance reduction and continuous high temperature operation to +155 C. Mounting options for the device include through-hole, solder, welded, or bolt-on.

The device released today is optimized for electric vehicles (EV), hybrid electric vehicles (HEV), solar, and wind power applications. With dimensions of 50.8 mm by 50.8 mm by 21.5 mm, the IHXL-2000VZ-5A’s 2000 case size is the largest available for a composite inductor. The inductor features an effective filtering frequency range up to SRF (13.1 MHz for 2.2H), very low DCR down to 0.21 mΩ typical, and nominal inductance of 2.2 H, with additional inductance values to be offered in the future.

The IHXL-2000VZ-5A handles high transient current spikes without hard saturation. Packaged in a 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra low levels, the inductor is specified for an operating temperature range of -55 C to +155 C, with high resistance to thermal shock, moisture, and mechanical shock. The device is RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the IHXL-2000VZ-5A are available now, with lead times of 12 to 14 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH