MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology RCWH Thick Film Chip Resistors Deliver Power of 0.33 W in 0805 Size to Save Space, Reduce Component Counts and Costs

Devices Provide Over 2.5x the Power Density of Standard Resistors in 0805 Footprint


RCWH

Products mentioned:

RCWH
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — May 15, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of thick film surface-mount wraparound chip resistors with high power ratings of 0.33 W in the compact 0805 case size. Offering a power density over 2.5x higher than standard devices in this footprint, Vishay Dale RCWH series resistors are designed to save space and reduce component counts in telecommunications, computer, industrial, and consumer applications.

With their high power density, the devices released today can be used instead of larger high power components or multiple lower power devices in new or existing designs. This reduces board space requirements and placement costs, while enabling smaller and lighter end products. In addition, RCWH series resistors provide higher reliability than larger thick film devices by reducing the coefficient of thermal expansion (CTE) mismatch with the PCB, thereby lowering solder joint stress.

The RCWH series offers extremely low resistance values from 0.01 Ω to 0.976 Ω, tolerance down to 0.5 %, and TCR down to 100 ppm/C. RoHS-compliant and halogen-free, the resistors feature a protective metal glaze on high quality ceramic. They are optimized as current sensing resistors and shunts in DC/DC converters, voltage regulation modules, and inverters in cell phones, computers, air conditioners, and heat pumps.

Samples and production quantities of the RCWH are available now, with lead times of six to eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH