MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology WSBS8518…20 Power Metal Strip® Battery Shunt Resistor Offers Improved Accuracy, Consistent Contact Location

36 W Device Features Low Resistance Down to 50 µΩ, Two Sense Pins to Assist in PCB Mounting


WSBS

Products mentioned:

WSBS8518...20
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — May 24, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new Power Metal Strip® battery shunt resistor featuring two sense pins that offers a 36 W power capacity in the 8518 case size. With extremely low resistance values down to 50 µΩ, the Vishay Dale WSBS8518...20 increases accuracy and lowers costs compared to Hall Effect current sensing solutions, while its sense pins assist in PCB mounting and provide consistent contact point location.

The device released today features a proprietary processing technique that produces extremely low resistance values of 50 µΩ, 100 µΩ, 125 µΩ, and 250 µΩ. These low values allow for more accurate data to determine battery charge and discharge, thus helping designers meet specific customer battery management requirements for applications in gas, diesel, hybrid, and electric cars and trucks, as well as electric forklifts, UPS systems, and other heavy industrial applications.

The WSBS8518...20 features a solid metal manganese-copper alloy resistive element with low TCR (± 20 ppm/°C), and a welded terminal to element connection. The resistor offers low inductance values of < 5 nH, low thermal EMF down to < 1 µV/°C, and an operating temperature range of -65 °C to +170 °C. The device is RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the WSBS8518...20 are available now, with a lead time of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH