MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology AC Filtering Film Capacitors Deliver Extremely Stable Capacitance and ESR in High Humidity Environments

Robust Metallized Polypropylene Devices Withstand THB Testing


MKP1847H

Products mentioned:

MKP1847H AC Filtering
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — May 31, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of metallized polypropylene AC filtering film capacitors optimized for high humidity environments. The Vishay Roederstein MKP1847H is the industry’s first full-range AC filtering film capacitor series to withstand demanding temperature humidity bias (THB) testing — 85 C, 85 % RH for 1,000 hours at rated voltage — without altering its electrical characteristics.

The capacitors released today are designed to ensure extremely stable capacitance and ESR values over a long service life under harsh environmental conditions during operation. The robust devices are ideal for input and output filtering in outdoor renewable energy inverters and critical applications such as UPS for sensitive datacenters.

MKP1847H series capacitors feature segmented film and offer rated capacitance from 1 F to 35 F and low ESR down to 3 mΩ. The devices provide high ripple current capabilities up to 24.5 A and rated voltages of 250 VAC, 310 VAC, 350 VAC, and 480 VAC.

Samples and production quantities of the MKP1847H series are available now, with a lead time of 10 weeks.

Resources:

AC filtering film capacitors from Vishay

Check distributor stock on the Vishay website

Weekly updates: sign up for Vishay Newsfeed

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH