MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology RCWK0306 Thick Film Chip Resistors Deliver Increased Accuracy While Saving Space and Reducing Component Counts

With Power of 0.33 W in 0306 Size, Four-Terminal Devices Provide 3.3x the Power Density of Standard Resistors in Larger 0603 Footprint


RCWK

Products mentioned:

RCWK0306
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — June 26, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new series of thick film surface-mount chip resistors featuring four-terminal Kelvin connections and high power ratings of 0.33 W in the compact 0306 case size. Offering a power density over 3.3x higher than standard devices in the 0603 footprint, Vishay Dale RCWK0306 series resistors are designed to save space and reduce component counts in telecommunications, computer, industrial, and consumer applications.

With their high power density, the devices released today can be used instead of larger high power components or multiple lower power devices. This reduces board space requirements and placement costs, while enabling smaller and lighter end products. In addition, RCWK0306 series resistors provide higher reliability than larger thick film devices by reducing the coefficient of thermal expansion (CTE) mismatch with the PCB, thereby lowering solder joint stress.

The resistors’ four-terminal Kelvin connection enables greater measurement accuracy with extremely low resistance values from 0.01 Ω to 0.1 Ω, and tolerance of 1 %. RoHS-compliant and halogen-free, the devices feature a metal glaze thick film on high quality ceramic. They are optimized as current sensing resistors in DC/DC converters, voltage regulation modules, and inverters in cell phones, computers, air conditioners, and heat pumps.

Samples and production quantities of the RCWK0306 are available now, with lead times of six to eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH