New Vishay Intertechnology TMBS Rectifiers in MicroSMP Package Save Significant Space While Increasing Power Density and Improving Efficiency

1 A and 2 A Devices Feature Low 0.65 mm Profile and Forward Voltage Drop Down to 0.36 V


VPL
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
MALVERN, Pa. — July 19, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its offering of surface-mount TMBS Trench MOS Barrier Schottky rectifiers with 10 new 1 A and 2 A devices in the eSMP series MicroSMP (DO-219AD) package. Providing space-saving alternatives to Schottky rectifiers in the SOD123W, the Vishay General Semiconductor devices feature reverse voltages from 45 V to 150 V and include the industry’s first 2 A TMBS rectifiers in the MicroSMP to deliver forward voltage as low as 0.40 V.

Currently, Schottky rectifiers with current ratings to 2 A are typically available in the SOD123W and SMA packages. The devices released today increase power density by offering this high forward current in the smaller MicroSMP. Measuring 2.5 mm by 1.3 mm with a low 0.65 mm profile, the package is 35 % thinner than the SOD123W, while occupying 45 % less board space. For excellent thermal performance, the MicroSMP features an asymmetric leadframe design.

With their forward voltage drop down to 0.36 V for 1 A devices and 0.40 V for 2 A devices, the rectifiers reduce power loss and improve efficiency in low voltage, high frequency inverters, DC/DC converters, and freewheeling and polarity protection diodes for commercial and industrial applications. The devices are also available in an AEC-Q101 qualified version for automotive applications.

The new rectifiers feature a maximum operation junction temperature up to +175 C and an MSL moisture sensitivity level of 1, per J-STD-020, LF maximum peak of +260 C. Ideal for automated placement, the devices are RoHS-compliant and halogen-free.

Device Specification Table:

Part # IF(AV) (A) VRRM (V) IFSM (A) VF at IF and TJ TJ max.(C)
VF(V) IF(A) TA(C)
V1P6 1 60 25 0.45 1 +125 +150
V2P6 2 60 30 0.51 2 +125 +150
V1PL45 1 45 25 0.36 1 +125 +150
V2PL45 2 45 30 0.40 2 +125 +150
V1PM10 1 100 25 0.58 1 +125 +175
V2PM10 2 100 30 0.62 2 +125 +175
V1PM12 1 120 25 0.61 1 +125 +175
V2PM12 2 120 30 0.65 2 +125 +175
V1PM15 1 150 25 0.64 1 +125 +175
V2PM15 2 150 30 0.68 2 +125 +175

Samples and production quantities of the new TMBS rectifiers are available now, with lead times of 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TMBS is a registered trademark of Vishay Intertechnology