MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology Extends OSOP Series of SMD Dual in-Line Thin Film Resistor Networks With New 16-Pin and 24-Pin Versions

Available With Isolated, Last Pin Common, and Custom Schematics in 25 mil Pitch QSOP Package, Devices Offer Tight Ratio Tolerances to 0.025%


ForOSOP

Products mentioned:

OSOP
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Aug. 2, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company has extended its OSOP series of surface-mount dual in-line thin film resistor networks in the 25 mil pitch QSOP package with new 16-pin and 24-pin versions in accordance with JEDEC MO-137, variation AB and AE. Available in isolated, last pin common, and custom schematics, the Vishay Dale Thin Film networks feature tight ratio tolerances to 0.025 % and low TCR tracking of 5 ppm/C to deliver higher precision than competing devices.

Optimized for precision voltage dividers and operational amplifiers, the resistor networks released today feature a low 1.73 mm maximum seated height, while their 25 mil pitch allows designers to reduce board space requirements by more than 50 % over current pitch standards. Typical applications will include telecommunications, industrial, process control, and medical instrumentation.

In isolated schematics, the 16-pin and 24-pin networks are available with 8 or 12 resistors, respectively, each with resistance values from 500 Ω to 100 kΩ and power ratings to 100 mW. In last pin common schematics, the devices are offered with 7 or 11 resistors. Featuring a rugged molded case construction with no internal solder, the networks provide absolute TCR of 25 ppm/ C and ratio stability of 0.015 % for 2,000 hours at 70 C.

The devices feature extremely low noise of < -30 dB and voltage coefficients of < 0.1 ppm/V, and they operate over a wide temperature range of -55 C to +125 C. The OSOP series is RoHS-compliant and halogen-free.

Samples and production quantities of the new resistor networks are available now, with lead times of 5 to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH