MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

New Vishay Intertechnology Rotational Absolute Magnetic Encoder Displacement Sensor: Higher Durability, Reliablity Over Hall Effect Potentiometers

Vishay Sfernice RAME027 Provides Accuracy of 0.33 % at 25 C in 27 mm Form Factor


RAME

Products mentioned:

RAME027
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

MALVERN, Pa. — Aug. 9, 2017 — Vishay Intertechnology, Inc. (NYSE:VSH) today introduced a new magnetic position sensor that delivers accuracy comparable to Hall effect devices while offering higher reliability and better durability. The one-time programmable (OTP) Vishay Sfernice RAME027 provides accuracy of 0.33 % at 25 C in a small 27 mm form factor. Typical applications will include military and industrial joysticks, electrical actuators, machine tools, textile manufacturing, milling, and robotics.

The robust capabilities and construction of the RAME027 make it the ideal solution for rough working conditions, including high vibration and shocks. Vishay can customize the RAME027 with customer-specified mechanical dimensions, output SSIs, accuracy and resolution levels, reinforcements, and protection features against EMC and ESD. Vishay can also provide redundant functions and an extended temperature range.

The RAME027 works from a 5 V ( 0.25 V) voltage supply and draws < 20 mA at 5 V. The device features a useful electrical angle of 360, an analog output, 12-bit resolution, and works over a temperature range of -25 C to +85 C.

Samples and production quantities of the RAME027 are available now, with a lead time of 16 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: