MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology ENYCAP Electrical Double-Layer Energy Storage Capacitors Offer Extended Capacitance Values in Additional Case Sizes

Available in Power and Energy Versions, Devices Offer Power Density to 4.1 Wh/kg and Capacitance From 15 F to 60 F


For220EDLCENYCAP

Products mentioned:

220 EDLC ENYCAP™
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Aug. 16, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced an extension to its 220 EDLC ENYCAP series of electrical double-layer energy storage capacitors for energy harvesting, power backup, and UPS power source applications. Available in power and energy versions with high stability, the Vishay BCcomponents devices now deliver a wider range of capacitance values in eight small case sizes ranging from 16 mm by 20 mm to 18 mm by 40 mm.

For the industrial, telecom, and PC markets, the polarized, energy storage capacitors released today offer high power density to 4.1 Wh/kg, capacitance values from 15 F to 60 F, and a rated voltage of 2.7 V at +65 C. 220 EDLC ENYCAP series devices feature very low internal resistance and rapid charge and discharge performance. The through-hole capacitors offer long leads and are RoHS-compliant.

Device Specification Table:

Version Energy Power
Capacitance (F) 15 to 55 20 to 60
Max. peak current @ +65 C (A) 25 25 to 35
Leakage current after 0.5 h (mA) 6 to 25 8 to 30
Stored energy at +65 C (Wh) 0.015 to 0.056 0.020 to 0.061
Specific energy +65 C (Wh/kg) 2.5 to 3.5 3.4 to 4.1

Samples and production quantities of the 220 EDLC ENYCAP series are available now, with lead times of six to eight weeks for larger quantities.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

ENYCAP is a trademark of Vishay Intertechnology

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH