MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology Launches Industry-First High Frequency IHLP® Inductor Series, Boosting DC/DC Efficiency

IHLP-1616BZ-0H Devices Feature High Frequency Performance Up to 10 MHz with Lowest Losses of Any Composite Inductor at 1 MHz and Above


IHLP

Products mentioned:

IHLP-1616BZ-0H
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Sept. 14, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the first extended-frequency inductor in the low profile, high current IHLP® family. The new IHLP-1616BZ-0H series features high frequency performance up to 10 MHz with the lowest losses of any inductor on the market for frequencies of 1 MHz and above. By using the IHLP-1616BZ-0H, designers can improve efficiency and potentially reduce the size of DC/DC converter circuitry.

Typical applications for the IHLP-1616BZ-0H will include notebook and desktop computers, sensors, cameras, POL converters, and various battery powered devices that require one or more regulated voltages. Working in conjunction with high frequency controller ICs, the IHLP-1616BZ-0H allows lower inductance values and thus lower DC losses as well as reduced high frequency core losses, enabling a physically smaller size of inductor to be used while boosting energy efficiency.

The IHLP-1616BZ-0H series features a typical DCR from 5.5 mµ to 26.6 mµ and inductance values from 0.10 µH to 1.0 µH. The IHLP-1616BZ-0H provides rated current to 45.0 A and handles high transient current spikes without saturation.

Packaged in a 100 % lead (Pb)-free shielded, composite construction that reduces buzz noise to ultra low levels, the inductor offers high resistance to thermal shock, moisture, and mechanical shock. The IHLP-1616BZ-0H is RoHS-compliant, halogen-free, and Vishay Green.

Device Specification Table:

Case size 1616
Profile (mm) 2.0
Inductance range (µH) 0.10 to 1.0
DCR typ. (mΩ) 5.5 to 26.6
DCR max. (mΩ) 5.9 to 28.5
Heat rating current (A) 6.1 to 14.0
Saturation current (A) 13.0 to 45.0
SRF typ. (MHz) 91 to 485

Samples and production quantities of the new inductor series are available now, with lead times of 10 to 12 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE
  • lang-code-JP
  • lang-code-ZH