New Vishay Intertechnology 25 V N-Channel Power MOSFET Offers Industry-Low On-Resistance for Increased Efficiency and Power Density

Device Features Maximum On-Resistance of 0.58 mΩ at 10 V and Low Gate Charge of 61 nC in Compact PowerPAK SO-8 Single Package


SiRA20DP

Products mentioned:

SiRA20DP
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
MALVERN, Pa. — Nov. 27, 2017 —Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 25 V n-channel TrenchFET Gen IV power MOSFET that features the industry’s lowest maximum on-resistance for such a device: 0.58 mΩ at 10 V. Delivering increased efficiency and power density for a wide range of applications, the Vishay Siliconix SiRA20DP offers the lowest gate charge and gate charge times on-resistance figure of merit (FOM) for devices with on-resistance below 0.6 mΩ.

Offered in the 6 mm by 5 mm PowerPAK SO-8 package, the device released today is one of the only two 25 V MOSFETs in the world with maximum on-resistance below 0.6 mΩ. In comparison, the SiRA20DP offers lower typical gate charge of 61 nC and a 32 % lower FOM of 0.035 Ω*nC. All other 25 V n-channel MOSFETs feature on-resistance that is 11 % higher or more.

The SiRA20DP’s low on-resistance minimizes conduction power losses to improve system efficiency and enable higher power density, which is ideal for OR-ring functions in redundant power architectures. The device’s low FOM enhances switching performance for DC/DC conversion in telecom and server power supplies, battery switching in battery systems, and load switching for 5 V to 12 V input rails.

The MOSFET is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.

Samples and production quantities of the SiRA20DP are available now, with lead times of 15 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.