MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology’s T59 Series of vPolyTan™ Low ESR Polymer Capacitors Named as 2017 ACE Awards Finalist


ACEAwards

Products mentioned:

T59
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

MALVERN, Pa. — Nov. 30, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its T59 series of vPolyTan™ multi-anode polymet surface-mount chip capacitors has been chosen as a 2017 ACE (Annual Creativity in Electronics) Awards finalist. The awards program, sponsored by EE Times and EDN magazine, recognizes “the best of the best in today’s electronics industry, including the hottest new products, start-up companies, design teams, executives, and more. “In the category of Passive, interconnects and Electromechanical,” the T59 series was selected as one of the three finalists.

Vishay’s T59 series capacitors deliver up to 25 % better volumetric efficiency than similar devices to provide the industry’s highest capacitance density, which in turn allows designers to reduce component counts, save PCB space, and lower overall solution costs. For example, their capacitance of 150 F at 30 V is three times higher in capacitance than the closest competing device. In addition, the capacitor’s patented multi-array packaging (MAP) ensures ultra low ESR from 25 mΩ to 150 mΩ at 25 C and 100 kHz.

Available in the molded EE (7343-43) case code, the devices offer capacitance from 15 F to 470 F, with capacitance tolerance of 20%, and overvoltage ratings up to 75 V. The T59 series features ripple current up to 3.1 A at 100 kHz and an operating temperature range of -55 C to +105 C. The capacitors are optimized for decoupling, smoothing, filtering and energy storage applications in sold-state drives, networking equipment, power supplies, and motherboards.

ACE Award winners will be announced at a ceremony taking place on December 6 at the San Jose Convention Center during ESC Silicon Valley.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager
Phone:  +49 9287 712 808 
Fax:  +49 9287 712 809 
E-mail:  paul.harrison@vishay.com

Sales contact: