MENU
< Back  

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

Vishay Intertechnology’s T59 Series of vPolyTan Low ESR Polymer Capacitors Honored With 2017 ACE Award


ACEAwards2017WINNERS

Products mentioned:

T59
For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in:

MALVERN, Pa. — Dec. 12, 2017 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its T59 series of vPolyTan multi-anode polymer surface-mount chip capacitors has been recognized with a 2017 ACE (Annual Creativity in Electronics) Award. The awards program, sponsored by EE Times and EDN magazine, recognizes leading companies, products and people in today's electronics industry. The T59 series was selected as the winner in the category of Passive, Interconnects and Electromechanical.

Vishay’s T59 series capacitors deliver up to 25 % better volumetric efficiency than similar devices to provide the industry’s highest capacitance density, which in turn allows designers to reduce component counts, save PCB space, and lower overall solution costs. For example, their capacitance of 150 F at 30 V is three times higher than the closest competing device. In addition, the capacitors’ patented multi-array packaging (MAP) ensures ultra low ESR from 25 mΩ to 150 mΩ at +25 C and 100 kHz.

Available in the molded EE (7343-43) case code, the devices offer capacitance from 15 F to 470 F, with capacitance tolerance of 20 %, and overvoltage ratings up to 75 V. The T59 series features ripple current up to 3.1 A at 100 kHz and an operating temperature range of -55 C to +105 C. The capacitors are optimized for decoupling, smoothing, filtering, and energy storage applications in solid-state drives, networking equipment, power supplies, and motherboards.

ACE Award winners were announced on Dec. 6 in a ceremony at the San Jose Convention Center during ESC Silicon Valley.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

vPolyTan is a trademark of Vishay Intertechnology.

For more information:
Media contact -  Paul Harrison, Senior MarCom Manager, Vishay Intertechnology Inc.
Phone:  +49-9287-712808 
Fax:  +49-9287-712809 
E-mail:  paul.harrison@vishay.com

Sales contact: 

This release in: