Next-Generation Vishay Intertechnology Miniature IR Receivers Provide Improved Sensitivity, Noise Suppression, and Pulse-Width Accuracy

For Remote Control Applications, New Devices Offer Increased Robustness to Optical and RF Emissions Without Sacrificing Sensitivity
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
MALVERN, Pa. — March 21, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the next generation of the company’s miniature infrared (IR) receiver modules for IR remote control applications. Devices in the Vishay Semiconductors TSOP11xxx, TSOP12xxx, TSOP13xxx, TSOP14xxx, and TSOP18xxx families deliver both improved dark-ambient and disturbed-ambient sensitivity to infrared signals, as well as better suppression of RF noise. The devices’ excellent pulse-width accuracy makes them suitable for codes demanding even the tightest pulse-width specifications, such as SIRCS and RCMM.

The receivers released today are designed for IR remote control in televisions, set-top boxes (STBs), audio systems, air conditioners, video projectors, cameras, video game systems, and more. For the remote control function in these products, the devices provide increased robustness against disturbances such as IR emissions from CFL lamps and RF emissions from on-board Wi-Fi antennas. In addition, the modules’ improved pulse-width accuracy allows lower bit error rates for almost any code, and the devices are insensitive to supply voltage variations and ripple noise.

To simplify designs, the receivers feature a photodetector, preamplifier circuit, and IR filter in a single 3-pin epoxy Cast (TSOP11xxx), Mold (TSOP12xxx and TSOP14xxx), Minimold (TSOP13xxx), or Minicast (TSOP18xxx) package. Each family is available with carrier frequencies from 30 kHz to 56 kHz and six automatic gain control (AGC) versions for short and long burst codes. All receivers feature a supply voltage from 2.5 V to 5.5 V and low supply current, and are RoHS-compliant, halogen-free, and Vishay Green.

Samples and production quantities of the new IR receiver modules are available now, with lead times of four to six weeks.

For the latest in all things opto — articles, videos, and products — visit Vishay's Opto Squad blog site: www.vishayopto.com.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.