MENU
< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Introduces IrDA-Compliant IR Transceiver Module in Standard 6.8 mm by 2.8 mm by 1.6 mm Footprint

Device Provides Drop-in Replacement for Parts From Other Manufacturers, Eliminating the Need for PCB Redesigns


Products mentioned:

TFBR4650
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa.Nov. 26, 2018 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company is providing designers with a new device for IrDA-compliant infrared (IR) transceiver modules in the standard 6.8 mm by 2.8 mm by 1.6 mm footprint. Vishay Semiconductor’s TFBR4650 offers a reliable drop-in replacement for devices from other manufacturers. In cases of discontinuation of competitors’ parts, this drop-in replacement prevents any need for PCB redesigns.

The device introduced today consists of a PIN photodiode, infrared emitter, and control IC in a single package. Compliant with the latest IrDA physical layer standard for IR data communication, the module supports data rates from 9.6 kbit/s to 115.2 kbit/s (SIR) for wireless transmission in gas and power meters, cell phones, microphones, robots, and mobile medical devices.

The TFBR4650 features a link distance up to 30 cm with standard IrDA and up to 20 cm with low power IrDA. The low power specification can be increased to 50 cm using an external resistor to set the emission intensity. Providing low power consumption, the module offers an idle supply current of 75 μA at 3.6 V and a shutdown current of 10 nA typical at +25 C. Lead (Pb)-free and RoHS-compliant, the device operates from 2.4 to 3.6 V over a temperature range of -25 C to +85 C.

Samples and production quantities of the new IR transceiver module are available now, with lead times of eight weeks.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-ZH
  • lang-code-JP
  • lang-code-DE