MENU
< Back  

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

Vishay Intertechnology Miniature IR Receivers in Heimdall and Panhead Packages Deliver Improved Sensitivity, Noise Suppression, and Pulse-Width Accuracy

New Devices Offer Increased Robustness to Optical and RF Emissions for Remote Control Applications


For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

MALVERN, Pa.May 29, 2019 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced two new series of miniature infrared (IR) receiver modules for IR remote control applications. Devices in the Vishay Semiconductors TSOP95xxx and TSOP96xxx series deliver improved dark-ambient and disturbed-ambient sensitivity to infrared signals, better suppression of RF noise, and excellent pulse-width accuracy.

The receivers released today are designed for IR remote control in televisions, set-top boxes (STBs), audio systems, air conditioners, video projectors, cameras, video game systems, and more. For the remote control function in these products, the devices provide increased robustness against disturbances such as IR emissions from CFL lamps and RF emissions from on-board Wi-Fi antennas. In addition, the modules’ improved pulse-width accuracy allows lower bit error rates for almost any code, and the devices are insensitive to supply voltage variations and ripple noise.

To simplify designs, the receivers feature a photodetector, preamplifier circuit, and IR filter in a single 4-pin epoxy Heimdall (TSOP95xxx) and Panhead (TSOP96xxx) package. The devices are available with carrier frequencies from 30 kHz to 56 kHz and five automatic gain control (AGC) versions for short and long burst codes. The receivers feature a low supply voltage from 2.0 V to 3.6 V and a typical supply current of 0.37 mA. They are RoHS-compliant, halogen-free, and Vishay Green.

Links to product datasheets on the Vishay website:

http://www.vishay.com/ppg?82837  (TSOP952.., TSOP954..)

http://www.vishay.com/ppg?82838  (TSOP953.., TSOP955..)

http://www.vishay.com/ppg?82839  (TSOP956..)

http://www.vishay.com/ppg?82847  (TSOP962.., TSOP964..)

http://www.vishay.com/ppg?82848  (TSOP963.., TSOP965..)

http://www.vishay.com/ppg?82849  (TSOP966..)

Samples and production quantities of the new IR receiver modules are available now, with lead times of four to six weeks.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

This release in:

  • lang-code-EN
  • lang-code-DE