Vishay Intertechnology 80 V MOSFET Offers Best in Class On-Resistance Times Gate Charge FOM to Increase Efficiency
Offered in PowerPAK® SO-8 Single Package, Device Combines On-Resistance Down to 2.35 mΩ With 55 nC Gate Charge and COSS of 614 pF

Products mentioned:
SiR680ADPMedia Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/
MALVERN, Pa. — Jan. 29, 2020 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 80 V TrenchFET® Gen IV n-channel power MOSFET in the 6.15 mm by 5.15 mm PowerPAK® SO-8 single package. Designed to save energy by increasing the efficiency of power conversion topologies and switching circuitry, the Vishay Siliconix SiR680ADP offers best in class on-resistance times gate charge — a key figure of merit (FOM) for MOSFET’s used in power conversion applications — of 129 mΩ*nC.
The device released today combines on-resistance down to 2.35 mΩ typical at 10 V with ultra low gate charge of 55 nC and COSS of 614 pF. These specifications are fine-tuned to reduce the power losses from switching, channel conduction, and diode conduction, resulting in increased efficiency. The MOSFET’s on-resistance times gate charge FOM is 12.2 % lower than the closest competing product and 22.5 % lower than the previous-generation device, making it the most efficient solution available for typical 48 V input to 12 V output DC/DC converters.
The SiR680ADP will serve as a building block in a wide variety of DC/DC and AC/DC conversion applications such as synchronous rectification, primary-side switching, buck-boost converters, resonant tank switching converters, and the OR-ing function in systems such as telecom and data center server power supplies; solar micro-inverters; motor drive control in power tools and industrial equipment; and battery switching in battery management modules.
The MOSFET is 100 % RG- and UIS-tested, RoHS-compliant, and halogen-free.
Samples and production quantities of the SiR680ADP are available now, with lead times of 12 weeks.
Vishay manufactures one of the world’s largest portfolios of discrete semiconductors and passive electronic components that are essential to innovative designs in the automotive, industrial, computing, consumer, telecommunications, military, aerospace, and medical markets. Serving customers worldwide, Vishay is The DNA of tech.® Vishay Intertechnology, Inc. is a Fortune 1,000 Company listed on the NYSE (VSH). More on Vishay at www.vishay.com.
https://www.facebook.com/VishayIntertechnology
###
TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.
Media Contact - Bob Decker, Redpines
Phone: 1.415.409.0233
E-mail: bob.decker@redpinesgroup.com
Sales Contact: http://www.vishay.com/
en/company/contacts/