Vishay Intertechnology to Highlight Power Components for SMPS, Wind Turbines, Electricity Meters, and More at PCIM Europe
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
MALVERN, PENNSYLVANIA — April 26, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) has announced that it will be highlighting its latest power capacitors, inductors, and diodes for high-current power converters, wind turbines, electricity meters, and many other applications at PCIM Europe 2010, being held May 4 to 6 in Nuremburg, Germany.

At the Vishay exhibit at Hall 12, Stand 344, product highlights will include Vishay Dale IHLP® inductors and shunt resistors for current sensing, Vishay ESTA power capacitors, and Vishay Semiconductors PowerBridge™ rectifiers and Trench MOS Barrier Schottky (TMBS®) diodes. In addition, Vishay will make two 20-minute presentations at the Trade Fair Forum in Hall 12, Stand 377 on its current shunt resistors (May 4 at 12:40 p.m.) and power resistors for wind turbines (May 5 at 10:30 a.m.).

Featured Vishay products at PCIM 2010:

Vishay Dale IHLP-6767DZ-01 inductor: This low-profile, high-current inductor in the 6767 case size features an ultra-low 4.0-mm profile, saturation currents up to 92 A, and standard inductance values from 0.22 μH through 10.0 μH. With a frequency range up to 2.0 MHz, the new IHLP-6767DZ-01 serves as a high-performing, space- and power-saving solution for voltage regulator module (VRM) and dc-to-dc applications in a wide range of end products.

Vishay Dale WSMS and WSBS Power Metal Strip® shunt resistors: With resistance values ranging from 0.00002 Ω to 0.001Ω and maximum current ratings up to 1000 A, these high-current devices are suited for applications such as battery monitoring and charge/discharge cycle control as well as for current measurement in industrial and home digital electricity meters.

Vishay ESTA HDMKP and EMKP high-current capacitors: The new HDMKP power capacitors support currents of up to 120 A and are ideally suited for power electronics applications such as industrial and traction converters, as well as converters for wind power installations, where they provide a higher than normal reliability and a lifetime expectancy of more than 100,000 operating hours (at rated voltage and hot spots below 70 °C). The new EMKP power capacitors have been designed for DC and AC applications with non-sinusoidal currents and voltages. Among their specific benefits are extremely low losses at higher frequencies, ESR values down to less than 4 mΩ, maximum currents of up to 80 A as well as high resilience under pulse loads and switching loads. The power capacitors are shock- and vibration-resistant and are extremely reliable, providing an operating life of more than 180,000 hours / 100 FIT. Available voltage ratings range from 400 V to 2400 V.

For more information on PCIM Europe 2010, visit http://www.mesago.de/en/PCIM/main.htm.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

IHLP and Power Metal Strip are registered trademarks of Vishay Dale Electronics, Inc. PowerBridge is a trademark of Vishay Intertechnology, Inc. TMBS is a registered trademark Vishay Intertechnology, Inc.