New 600 V, 47 A Vishay Siliconix N-Channel Power MOSFET Features Industry’s Best FOM of 15.12 Ω-nC, and On-Resistance of 0.07 Ω in TO-247 Package


SiHG47N60S mosfets

Products mentioned:

SiHG47N60S
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
MALVERN, PENNSYLVANIA — Nov. 4, 2010 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new 600 V, 47 A n-channel power MOSFET with ultra-low maximum on-resistance of 0.07 Ω at a 10 V gate drive and an improved gate charge of 216 nC in the TO-247 package. The SiHG47N60S’s 15.12 Ω-nC gate charge times on-resistance, a key figure of merit (FOM) for MOSFETs used in power conversion applications, is the industry’s lowest for this device type.

The low on-resistance of the SiHG47N60S translates into lower conduction losses that save energy in inverter circuits and pulsewidth modulation (PWM) full-bridge topologies in solar and wind inverters, and telecom, server, and motor control power applications.

The new SiHG47N60S is produced using Vishay Super Junction technology, which has been tailored to minimize on-state resistance and withstand high energy pulse in the avalanche and commutation mode. The MOSFET is compliant to RoHS Directive 2002/95/EC and 100% avalanche tested for reliable operation.

Samples and production quantities of the new power MOSFET are available now, with lead times of 10 to 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.