Vishay Siliconix 8 V P-Channel TrenchFET® Power MOSFET Offers Industry’s Lowest On-Resistance Down to 16 mΩ in PowerPAK® SC-70 2 mm by 2 mm Footprint Area


SiA427DJ
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
MALVERN, PENNSYLVANIA — Jan. 17, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced a new 8 V p-channel TrenchFET® power MOSFET with the lowest on-resistance ever achieved for a p-channel device in the thermally enhanced PowerPAK® SC-70 2 mm by 2 mm footprint area.

The SiA427DJ offers an ultra-low on-resistance of 16 mΩ at 4.5 V, 26 mΩ at 1.8 V, 32 mΩ at 1.5 V, and 95 mΩ at 1.2 V. The closest competing device is a 20 V p-channel power MOSFET, with an 8 V gate-to-source rating, offering on-resistance of 25.8 mΩ at a 4.5 V gate drive, 41.1 mΩ at 1.8 V, and 63.2 mΩ at 1.5 V. These values are 36 %, 37 %, and 47 % higher, respectively, than the SiA427DJ. Compared to a typical device in the standard SC-70 package, occupying the same PCB area, the PowerPAK SC-70 can handle 40 % more power dissipation under the same ambient conditions.

The ultra-small PowerPAK SC-70 package of the SiA427DJ is optimized for small handheld electronics. The new device will be used for load switches in portable devices such as cell phones, smart phones, MP3 players, digital cameras, eBooks, and tablet PCs.

For these devices, the lower on-resistance of the SiA427DJ translates into lower conduction losses, thus prolonging battery life between charges. The device’s low on-resistance rating of 1.2 V is ideal for low bus voltages. Applications using a 1.2 V power bus will also benefit from the MOSFET’s low on-resistance at 1.5 V and 1.8 V as power line voltages fluctuate, allowing the SiA427DJ to provide the best overall power savings.

100 % Rg tested, the MOSFET is halogen-free in accordance with IEC 61249-2-21 and compliant to RoHS directive 2002/95/EC.

Samples and production quantities of the new SiA427DJ TrenchFET power MOSFET are available now, with lead times of 12 to 14 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.