Vishay Intertechnology’s New USB-OTG Bus Port Protection Array Provides Low Typical Capacitance of 0.7 pF and Low Maximum Leakage Current Down to 0.085 A in Compact LLP75-7L Leadless Package

Device Provides V BUS Protection at 28 V Working Range


VBUS053CZ-HAF usbprotection

Products mentioned:

VBUS053CZ-HAF
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
MALVERN, Pa. — Jan. 24, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new ESD-protection array featuring low capacitance and leakage currents to protect USB-OTG ports against transient voltage signals. The new VBUS053CZ-HAF provides three lines of USB ESD protection at a 5.5 V working range, and one line of VBUS protection at a 28 V working range.

The VBUS053CZ-HAF is packaged in the leadless LLP75-7L package, with an ultra-low profile of 0.6 mm to minimize the board space required for active ESD protection in high-speed data applications, such as USB 2.0 and HDMI in HDTVs and mobile electronics, including portable gaming systems, MP3 players, and cell phones.

The new device features a low load capacitance of 0.7 pF for the three data lines D+, D-, and ID, and a low maximum leakage current of 0.085 A at the working voltage of 3.3 V, and 1 A at 5.5 V. The array provides a low typical clamping voltage of 15 V at 3 A for the data lines. For the VBUS line, the VBUS053CZ-HAF features a typical clamping voltage of 53 V at 3 A.

The VBUS053CZ-HAF provides transient protection as per IEC 61000-4-2 at 15 kV contact and 15 kV air discharge as well as surge current protection in accordance with IEC 6100-4-5 from 3 A.

The lead (Pb)-free device features a halogen-free molding compound, and is compliant with RoHS 2002/95/EC and WEEE 2002/96/EC.

Samples of the new USB-OTG bus port protection array are available now, with lead times of six to eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.