Vishay Intertechnology’s T97 and 597D Solid Tantalum Chip Capacitors and SiR880DP ThunderFET® 80 V N-Channel Power MOSFET Named as Design News Golden Mousetrap Best Product Finalists


mousetrap

Products mentioned:

T97
597D
SiR880DP
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
MALVERN, PENNSYLVANIA — March 29, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that its Tantamount® Hi-Rel COTS T97 and commercial, industrial-grade 597D series of solid tantalum chip capacitors, and ThunderFET® SiR880DP 80 V n-channel power MOSFET have been selected as 2011 Design News Golden Mousetrap Best Product finalists in the Electronics & Tests category.

For more than two decades, the Design News Awards Program has recognized engineering innovation and creativity in product design. This year, Golden Mousetrap awards were given in four major categories: Electronics & Test, Automation & Control, Design Tools: Hardware & Software, and Materials & Assembly. This year’s finalists were chosen by Design News editors from a record number of entries.

“The products highlighted in this year's Golden Mousetrap winners and finalists clearly demonstrate both cutting-edge design ideas and the practical evolution of technologies for systems and product design engineers. Design News congratulates all the engineers and their companies who have been recognized with the Golden Mousetrap Award, and we are grateful for their contribution to this year's competition,” said David Greenfield, editorial director at Design News.

Vishay’s Hi-Rel COTS T97 and commercial, industrial-grade 597D series are the industry’s first 75 V solid tantalum chip capacitors. The devices provide high reliability in circuits with applied voltages between 25 V and 40 V, a performance level that has previously been available only with through-hole technology. The T97 and 597D feature a capacitance range of 10 µF to 1500 µF, ESR down to 0.015 Ω at + 25 °C, and a voltage range from 4 V to 75 V in nine case sizes, including the “V” case with a low 2-mm profile. The T97 series offers designers a wide array of ratings not found in available MIL specifications, combining the flexibility and convenience of a commercial product with the reliability needed in demanding applications.

As the industry’s first 80 V power MOSFET to offer an on-resistance rating at a 4.5 V gate drive, Vishay’s ThunderFET SiR880DP allows for higher-frequency designs, while lowering costs by enabling the use of 5 V PWM ICs. The SiR880DP ’s very low on-resistance of 8.5 mΩ at 4.5 V, 6.7 mΩ at 7.5 V, and 5.9 mΩ at 10 V translates into reduced power consumption and greener solutions, especially at light loads such as stand-by mode. Typical on-resistance times gate charge, a key figure of merit (FOM, expressed in nC-mΩ) for MOSFETs in dc-to-dc converter applications, is 161 at 4.5 V.

A complete list of finalists can be found at designnews.com. Winners of the Golden Mousetrap Awards will be announced in Design News’ March issue, and will be featured in the magazine’s New Product Newsletters in the coming months.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

ThunderFET is a registered trademark of Siliconix incorporated. Tantamount is a registered trademark of Vishay Intertechnology, Inc.