Vishay Intertechnology Releases Industry’s First Submersible Cermet Panel Potentiometer With Full IP68 Sealing Against Deep Sea Water for Operation to 30 m (100 Feet)


110718potentiometers

Products mentioned:

P13SM
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
MALVERN, Pa. — July 18, 2011 — Vishay Intertechnology Inc. (NYSE: VSH) today announced a new submersible cermet panel potentiometer that is the industry’s first to be fully IP68 sealed against deep sea water. Featuring a stainless steel shaft and bushing, the P13SM is designed for applications where electrical parameters need to be set with an immersed potentiometer in deep sea salt water conditions up to 30 m (100 feet). The device achieves corrosion resistance times of up to 960 hours in a salt spray test.

Featuring a heavy-duty construction, the Vishay Sfernice potentiometer released today is optimized for use as a voltage divider operator interface for underwater equipment, submarine scooters, and lighthouses. The P13SM reduces costs by eliminating the need to design and build sealed protection against sea salt water for the device in these applications.

The P13SM offers a high power rating to 1.5 W at + 70 C and tight TCR of 75 ppm/C typical. The device’s cermet element provides better stability than carbon elements, and offers greater reliability and robustness.

The potentiometer is available in 3.17 mm and 6 mm shaft diameters, and multiple shaft lengths. The device offers a temperature range of - 55 C to + 125 C to ensure reliable operation even in extreme environments

Samples and production quantities of the new P13SM are available now, with lead times of 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.