Vishay Intertechnology Introduces Streaming Video Highlighting Vishay Dale LCD Displays on Web Site

Video Explores Demonstration Cases Featuring the Company’s Latest LCD Products


111003displays
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — Oct. 3, 2011 — To assist customers in selecting the best Vishay Dale LCD products for their applications, Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has added a new streaming video to its website (http://www.vishay.com) providing an overview of the complete portfolio using a series of demonstration cases which contain the company's latest LCD products.

Vishay provides a complete line of standard character and graphic LCD modules with integrated electronics and a wide variety of sizes, backlight colors, technologies, LCD modes, polarizers, temperature ranges, and viewing directions. The video introduced today explores five demonstration cases which showcase the latest additions to Vishay’s LCD offering.

The -06 case features the full line of active TFT color products, available in 2.8 in, 3.5 in, 4.3 in, and 5.7 in diagonal displays. The -05 case includes the largest variety of displays for the popular 16x2 character module, and contains chip-on-glass technology and monochrome quarter VGA displays in sizes to 5.7 in.

The -04 case contains all of Vishay’s graphic displays up to the quarter VGA size, while the -03 case offers character modules ranging in size from 8x2 to 10x4. The -02 case features 320x240 quarter VGA displays with diagonal sizes from 4 in to 6 in.

Vishay’s LCD products can be used with any user interface application requiring visual interaction. This includes gaming; avionics; instrumentation; industrial and commercial controllers; audio and digital equipment; military, automotive, and industrial equipment; agriculture; oil and petroleum products; medical equipment; consumer goods; and ATM applications.

If a standard product does not meet a customer’s design needs, Vishay’s engineering department offers its expertise to create a completely custom LCD glass, provide modifications to a standard module by adding a pigtail or header, or develop a full module to fit any application.

To view the video, go to:

http://www.vishay.com/videos/optoelectronics-displays/lcd-display-overview.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.