Vishay Intertechnology Increases Minimum Capacitance of VJ HVArc Guard® Surface-Mount X7R MLCCs up to 470 pF

C0G Dielectric Now Available for Lower Capacitance Values Down to 10 pF


VJ HVArc Guard

Products mentioned:

VJ HVArc Guard®
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
MALVERN, Pa. — Dec. 15, 2011 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it has increased the minimum capacitance values for its VJ HVArc Guard® surface-mount X7R multilayer ceramic chip capacitors (MLCCs). For lower capacitance values, the company offers a C0G (NP0) dielectric option with a voltage range of 1000 V to 2500 V in five case sizes from 0805 to 2225.

The minimum capacitance values for VJ HVArc Guard X7R MLCCs have increased to 470 pF in the 0805 case size, and 220 pF in the 1206, 1210, 1808, and 1812 case sizes. If lower capacitance is required, 1000 V X7R devices in the 0805, 1206, and 1210 case sizes can be replaced by C0G MLCCs, which offer a low minimum capacitance of 10 pF.

The VJ HVArc Guard devices feature a unique, worldwide patented internal design structure that prevents surface arc-over at high voltages. This design allows for higher capacitances than standard high-voltage MLCCs, and facilitates the use of smaller case sizes in high-voltage products, allowing for device miniaturization and reducing component cost.

The MLCCs are available with optional polymer terminations that provide increased resistance to board flex cracking. With these terminations, the devices reduce capacitor failures related to mechanical cracking, and save warranty costs by confining failures to the capacitor, thus reducing the number of damaged components on the circuit board or damage to the complete device itself.

Manufactured in Noble Metal Electrode Technology (NME) with a wet build process, VJ HVArc Guard MLCCs are optimized for high-voltage applications including buck and boost dc-to-dc converters and voltage multipliers for flyback converters in power supplies for cable modems and routers. The devices are compliant to RoHS Directive 2002/95/EC and halogen-free according to the IEC 61249-2-21 definition.

Device Specification Table:

Dielectric Case Voltage (V) Capacitance
Minimum Maximum
C0G (NP0) 0805 1000, 1500 10 pF 390 pF
1206 1000, 1500 10 pF 1.5 nF
1210 1000, 1500 10 pF 2.7 nF
2220 1000, 1500 470 pF 5.6 nF
2225 1000, 1500, 2500 470 pF 8.2 nF
X7R 0805 630, 1000 470 pF 3.3 nF
1206 250, 500, 630, 1000 220 pF 47 nF
1210 250, 500, 630, 1000 220 pF 82 nF
1808 250, 500, 630, 1000 220 pF 100 nF
1812 250, 500, 630, 1000 220 pF 270 nF

Samples and production quantities of the VJ HVArc Guard MLCCs are available now, with lead times of 10 to 14 weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

HVArc Guard is a registered trademark of Vishay Intertechnology.