Vishay Intertechnology’s New Power Metal Strip® Meter Shunt Resistor Features Very Low Resistance Values Down to 300 µΩ and 3 W Power Capability in 2906 Size Package


WSMS2906 metal strips
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
MALVERN, Pa. — Feb. 16, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new Power Metal Strip® meter shunt resistor that combines a 3 W power capability in the 2906 size package with very low resistance values down to 300 µΩ.

The WSMS2906 meter shunt resistor features a proprietary processing technique that produces extremely low resistance values from 300 µΩ to 660 µΩ. These values allow for increased accuracy in current meter shunt applications for industrial and consumer single- or multiphase energy meters. With a tolerance of 5.0 %, the new resistor provides power companies with more accurate data to determine customer usage and to adjust billing terms.

The WSMS2906 features a five-terminal connection design and an all-welded construction that contributes to its superior electrical performance. The resistor offers very low inductance values of < 5 nH and a low thermal EMF of < 3 µV/°C. The device is lead (Pb)-free and RoHS-compliant.

Samples and production quantities of the new meter shunt resistor are available now, with a lead time of eight to 10 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.