Vishay Intertechnology Launches Infrared Receivers Compliant to 3DTV CEA-2038 Command-Driven IR-Synchronized Active Eyewear Standard

Surface-Mount Receivers Feature 26.2 kHz Carrier Frequency Reception and 830 nm Peak Wavelength Sensitivity


TSOP75D26 TSOP35D26 modules

Products mentioned:

TSOP35D26
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
MALVERN, Pa. — March 19, 2012 — Addressing the high cost and lack of interoperability of active 3D glasses, Vishay Intertechnology, Inc. (NYSE: VSH) today released two infrared receivers developed specifically to be compliant with the Consumer Electronics Association’s CEA-2038 standard for IR synchronization of active eyewear used with 3DTV sets. The TSOP75D26 and TSOP35D26 are industry-first, surface-mount IR receivers designed to be assembled into active 3D glasses, where they receive infrared signals from the TV set and ensure the glasses’ LCD shutters open and close in proper synchronization to create the 3D effect. With these industry standard receivers, TV manufacturers can reduce the cost of the active 3D glasses, one of the main barriers to broader adoption of 3D TVs. With adoption of the CEA-2038 standard and use of the TSOP75- and TSOP35D26 receivers, consumers will be able to watch 3D programs on any TV set.

Per the standard, the receivers are designed to operate on a carrier frequency of 26.2 kHz, which is lower than that used by standard remote control systems and thus helps avoid possible interference from TV and set-top box remote controls. The TSOP75D26 and TSOP35D26 are also designed to receive the 3D synchronization signals from an 830 nm emitter, further avoiding the possibility of interference. They are compliant with the standard’s long encoding command sequence which features better immunity in noisy environments. Like all of Vishay’s IR receivers, the TSOP75D26 and TSOP35D26 feature industry-leading suppression of optical noise from compact fluorescent lights, LCD backlights, and plasma panels.

The TSOP75D26 and TSOP35D26 integrate a photodiode, amplifier, automatic gain control, band pass filter, demodulator, and control IC into a single tiny package which helps minimize the weight of 3D glasses, while their ultra-low current consumption maximizes the battery life. The TSOP75D26 and TSOP35D26 are surface-mount devices that can be mounted in a side or top view. They both have a viewing angle of 50 which allows for significant head movement without signal loss. The TSOP75D26 measures 2.3 mm x 3.0 mm x 6.8 mm and has dual lenses while the TSOP35D26 measures 4.0 mm x 5.3 mm x 7.5 mm and has a single lens.

Samples of the new TSOP75D26 and TSOP35D26 are available now. Production orders have a lead time of six to eight weeks.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.