Vishay Intertechnology Launches PowerCAD On-Line Simulation Tool for Point-of-Load DC/DC Circuits


PowerCAD Simulation tool

Products mentioned:

SiC401A, SiC401BCD
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
MALVERN, Pa. — March 21, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the PowerCAD Simulation tool, a free on-line tool that gives engineers a fast and convenient way to test and optimize DC/DC circuits built with Vishay Siliconix regulator ICs.

Using an intuitive interface, the PowerCAD Simulation tool supports both experienced analog and power designers as well as junior or digital designers with less experience in high-power, high-frequency voltage regulator design.

Based on the required operating conditions, the engineer can select the appropriate regulator from the Vishay product offering and generate a full circuit schematic for the application. The schematic can then be edited as required for more advanced users or for performance comparison purposes.

Once the basic circuit is created, the designer can perform DC, transient, and start-up simulations with visibility of all the circuit node waveforms. An efficiency analysis and optimization of the circuit with detailed power loss analysis may also be performed.

Following these steps, the PowerCAD Simulation tool generates a bill of materials (BOM) available for online ordering, allowing a quick validation that dramatically reduces design cycle times. The circuit simulation can also be shared easily with Vishay FAEs for additional technical support or any other related question.

Regulator ICs supported by the PowerCAD Simulation tool include the Vishay Siliconix microBUCK® family of fully protected high-efficiency, high-frequency step-down voltage regulators. Examples of regulator ICs supported by the tool include the SiC401A and SiC401BCD.

Providing high performance in a compact footprint, microBUCK serves as a cost-effective solution for a wide range of point-of-load (POL) applications having input voltages from 2.7 V to 36 V and handling up to 15 A of load current. The PowerCAD Simulation tool provides on-the-fly simulation for all of the following microBUCK devices: SiC413, SiC414, SiC424, SiC401, SiC402, SiC403, and SiP12107.

The Vishay PowerCAD Simulation tool joins the ThermaSim online thermal simulation tool, reference boards, and other online collateral as part of Vishay’s commitment to serving its worldwide customers as a one-stop shop for power management solutions.

The Vishay PowerCAD Simulation tool can be found at http://www.vishay.com/power-ics/powercad-list. A PowerCAD user’s guide is available at http://www.vishay.com/doc?49225.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

microBUCK is a registered trademark of Siliconix incorporated