Vishay Intertechnology Announces “Super 12” Featured Products for 2012

Innovative Components Offer Industry-Leading Specifications for a Variety of Applications
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
MALVERN, Pa. — March 26, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced its “Super 12” featured products for 2012. Each year, Vishay’s Super 12 collection showcases the company’s industry-leading capabilities in semiconductor and passive devices, providing design engineers with a short-cut to leading industry specs and a cross-section of Vishay’s very broad product portfolio.

The Super 12 products for 2012 are:

MKP1848S Film Capacitors - Slim metallized DC polypropylene film capacitors for DC-link applications feature the industry’s broadest CV range from 2 µF to 100 µF, voltage ratings from 500 VDC to 1,000 VDC, and low profiles of 12 mm, 15 mm, 18 mm, and 24 mm.

VCUT05D1-SD0 BiSy Single-Line ESD Protection Diode - Offered in the new ultra-compact CLP0603 silicon package, the diode provides low capacitance of 10 pF for signal and data line protection from transient voltage signals in portable electronics.

34 THE Non-Contacting Multi-Turn Sensor - The industry’s first multi-turn sensor to feature non-contacting technology, the 34 THE offers a very long life of 50 million cycles with a servo mount and 10 million cycles with a bushing mount, and is available with any electrical angle up to 3600° maximum.

45 V Trench MOS Barrier Schottky TMBS® Single-Chip Rectifiers - Feature a wide range of current ratings from 10 A to 40 A and extremely low forward voltage drops down to 0.51 V typical at 20 A. Optimized for use in solar cell junction boxes as bypass diodes.

MPM Matched Pair Resistor Network − Features tight ratio tolerance and close TCR tracking with divider ratios of 1:1 to 100:1 for process controls, test and measurement, instrumentation, signal conditioning, and data acquisition applications.

CNY6 Series CAT IV Optocouplers - The industry’s first such devices available in surface-mount packages and optimized for solar and wind turbine installations, the optocouplers protect equipment and people from being damaged or injured by a high-voltage spike or transient of up to 12,000 V and a recurring peak voltage of 1450 V while allowing data to pass from the high-voltage side to low-voltage monitoring equipment.

IHLP® 3232 Series Low-Profile, High-Current Inductors - High-performing, space- and power-saving solutions for voltage regulator module (VRM) and DC/DC converter applications in mobile devices, notebooks, desktop computers, servers, graphic cards, portable gaming systems, personal navigation systems, and more.

SiHG73N60E E Series 600 V High-Voltage MOSFET − Features on-resistance of 39 mΩ at a 10 V gate drive and ultra-low gate charge of 362 nC maximum for outstanding performance in SMPS, PFC, lighting, and industrial applications.

TM8 MicroTan® Tantalum Capacitor - For critical high-reliability medical and military-aerospace applications, the TM8 features very low DC leakage current in compact case sizes along with customizable screening options, including Weibull failure rate grading.

SiSA04DN 30 V MOSFET − Offered in the thermally advanced PowerPAK® 1212-8 package, this TrenchFET® Gen IV device features on-resistance down to 2.5 mΩ, gate charge down to 22.5 nC for a DC/DC conversion figure of merit (FOM) of 56.

TNPU e3 High-Precision Thin Film Chip Resistor - Combines reliability and an advanced level of precision — with tolerances as low as ± 0.05 % and TCR values down to ± 5 ppm/K — for amplifiers, precision voltage dividers, and control units in industrial, automotive, aerospace, medical, and telecommunications equipment.

SiP12107 / SiP121078 Scalable Step-Down Regulators − High-frequency current-mode constant on-time (CM-COT) synchronous buck regulators with integrated high-side and low-side power MOSFETs. Their power stage is capable of supplying 3 A or 5 A continuous current at a 4 MHz switching frequency for computing, consumer electronics, telecommunications, and industrial applications.

More information about Vishay’s Super 12 products is available at http://www.vishay.com/landingpage/super12/2012/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TMBS, IHLP, and MicroTan are registered trademarks of Vishay Intertechnology. TrenchFET and PowerPAK are registered trademarks of Siliconix incorporated.