Vishay Intertechnology Launches New Non-Zero Crossing Phototriac Optocouplers in Compact, Environmentally Green SOP-4 Package


VOM160 VOM160NT VOM160PT VOM160RT VOM305x VOM3053T VOM3052T optocouplers

Products mentioned:

VOM160
VOM3052, VOM3053
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
MALVERN, Pa. — June 11, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) is broadening its optoelectronics portfolio with the release of new non-zero crossing phototriac optocouplers in the industry-standard miniflat SOP-4 package, saving up to 66 % in PCB space compared to devices in the DIP-6 package.

The new VOM160 and VOM305x series offer three choices of input trigger LED current: 5 mA (VOM160NT / VOM3053T), 7 mA (VOM160PT), and 10 mA (VOM160RT / VOM3052T). With a package height of only 2.0 mm, they feature a blocking voltage of 600 V AC for high-voltage applications.

In consumer applications, the VOM160 and VOM305x series will be used for turning on and off motors and solenoid control in refrigerators, washers, lamps and coffee makers. The new devices will also be used to drive TRIACs for solid-state relays and static AC power switches in industrial applications.

The VOM3052T and VOM3053T, with their high static dV/dt of 1500 V/Ás, are particularly well suited for noisy environments where a lower dV/dt can cause a thyristor to be triggered as a result of a high slew rate transient on the output load, even without any triggering signal on the input.

Key specifications table

Device Trigger current IFT(mA) Minimum critical rate of rise off-state voltage dV/dt (V/μs) Maximum peak off-state voltage VDRM (V) Isolation test voltage VISO (VRMS)
VOM3053T 5 1500 600 3750
VOM3052T 10
VOM160NT 5 500
VOM160PT 7
VOM160RT 10

Samples and production quantities of the new VOM160NT, VOM160PT, VOM160RT, VOM3052T and VOM3053T are available now.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.