Vishay Intertechnology Releases New Series of Surface-Mount TransZorb® TVS in SlimSMA™ Package

Compact Devices Combine Ultra-Low 0.95 mm Profile With High Surge Capability to 600 W


SMA6F diodes

Products mentioned:

SMA6F5.0A thru SMA6F20A
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
MALVERN, Pa. — July 9, 2012 — Vishay Intertechnology, Inc. (NYSE:VSH) today introduced a new series of surface-mount TransZorb® transient voltage suppressors (TVS) in the SlimSMA™ DO-221AC package. SMA6F series devices offer a very low profile of 0.95 mm, high surge capability to 600 W at 10/1000 µs and 4 kW at 8/20 µs, and excellent clamping capability.

The TVS devices released today are 50 % thinner than devices in the traditional SMA package, yet are footprint compatible and offer 50 % higher surge capability at 10/1000 µs. The SMA6F series’ low clamping voltages of 9.2 to 31.4 at 10/1000 µs and 13.4 to 36.8 at 8/20 µs are 3 % to 9 % lower than current TVS devices in the SMB package.

With their compact size, SMA6F TVS are designed to protect sensitive electronics against voltage transients induced by inductive load switching and lightning in space-constrained consumer, computer, industrial, and telecommunication applications. Typical end products include hard disks, hot swap computer and telecom cards, and slim LCD TVs and monitors.

The SMA6F series consists of 16 TVS devices with stand-off voltages from 5 V to 20 V. The devices offer a temperature range from - 55 to + 175, provide ESD capability of 15 kV (air) and 8 kV (contact) in accordance to IEC 61000-4-2 Level 4, and meet the MSL Level 1 standard, per -STD-020, LF maximum peak of 260 °C.

Ideal for automated placement, the TVS devices are RoHS-compliant and halogen-free.

Samples and production quantities of the new SMA6F series are available now, with lead times of eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

SlimSMA is a trademark and TransZorb is a registered trademark of Vishay Intertechnology.