Vishay Intertechnology’s New 170 V TMBS® Rectifiers for Telecom Power Supplies Feature Current Ratings up to 80 A, Typical Forward Voltage Drop Down to 0.65 V
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
MALVERN, Pa. — Oct. 11, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today expanded its offering of TMBS® Trench MOS Barrier Schottky rectifiers with nine new 170 V devices in power TO-220AB, TO-263AB, and TO-3PW packages. Aimed at telecom power supply applications, the devices feature a wide range of current ratings, from 10 A to 80 A, and a typical forward voltage of 0.65 V at 30 A.

The new devices feature a dual center-tap configuration. They include the 10 A V10170C and VB10170C; the 40 A V40170C, VB40170C, and V40170PW; the 60 A V60170G, VB60170G, and V60170PW; and the 80 A V80170PW.

All nine devices feature a 175 °C maximum junction temperature. Devices in the TO-263AB package additionally feature an MSL moisture sensitivity level of 1, while devices in the TO-220AB and TO-3PW feature solder bath temperatures of 275 °C maximum and are halogen-free per the JEDEC JS709A definition.

Device Specification Table:

Vishay P/N IF
(A)
VRRM
(V)
VF at IF and TJ IFSM
(A)
Package
VF
(V)
IF
(A)
TA
(°C)
V10170C-M3 10 170 0.65 5 125 80 TO-220AB
VB10170C-E3 10 170 0.65 5 125 80 TO-263AB
V40170C-M3 40 170 0.68 20 125 200 TO-220AB
VB40170C-E3 40 170 0.68 20 125 200 TO-263AB
V60170G-M3 60 170 0.72 30 125 210 TO-220AB
VB60170G-E3 60 170 0.72 30 125 210 TO-263AB
V40170PW-M3 40 170 0.67 20 125 200 TO-3PW
V60170PW-M3 60 170 0.65 30 125 260 TO-3PW
V80170PW-M3 80 170 0.68 40 125 280 TO-3PW

Samples and production quantities of the new 170 V TMBS rectifiers are available now, with lead times of eight weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TMBS is a registered trademark of Vishay Intertechnology.