Vishay Intertechnology Releases New 45 V TMBS® Trench MOS Barrier Schottky Rectifiers in Low-Profile SlimSMA™ Package

High Current Density Devices Feature Forward Currents to 5 A and V F Down to 0.37 V


VSSAF3L45 VSSAF5L45 diodes

Products mentioned:

VSSAF3L45
VSSAF5L45
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
MALVERN, Pa. — Dec. 5, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced new 45 V TMBS® Trench MOS Barrier Schottky rectifiers offering high current density with forward currents of 3 A and 5 A in the surface-mount SlimSMA™ DO-221AC package featuring a low 0.95 mm profile.

With extremely low forward voltage drops down to 0.37 V typical at 3 A, the new VSSAF3L45 and VSSAF5L45 reduce power loss and improve efficiency in low-voltage, high-frequency DC/DC converters, freewheeling diodes, and polarity protection in space-constrained applications such as smartphone chargers.

The new rectifiers feature a maximum operation junction temperature of + 150 °C and an MSL moisture sensitivity level of 1, per J-STD-020, LF maximum peak of 260 °C. Ideal for automated placement, the devices are compliant to RoHS Directive 2011/65/EU and halogen-free according to JEDEC JS709A standards.

Device Specification Table:

Product category Vishay P/N IF
(A)
VRRM
(V)
VF(typ.) at IF and TJ IFSM
(A)
TJmax
(°C)
VF
(V)
IF
(A)
TA
(°C)
TMBS VSSAF3L45 3 45 0.37 3 125 80 150
VSSAF5L45 5 45 0.39 5 125 100

Samples and production quantities of the new 45 V TMBS rectifiers are available now, with lead times of four weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TMBS is a registered trademark of Vishay Intertechnology. SlimSMA is a trademark of Vishay Intertechnology.