Vishay Intertechnology’s New Power Metal Strip« Resistor Combines High 2 W Power Rating With Extremely Low Resistance Values Down to 0.001 Ω in 2010 Case Size


WSLP2010 resistor metalstrip

Products mentioned:

WSLP
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
MALVERN, Pa. — Dec. 20, 2012 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced a new surface-mount Power Metal Strip« resistor in the 2010 case size that combines a high 2 W power rating with extremely low resistance values down to 0.001 Ω and stable resistance tolerances to 0.5 %.

The advanced construction of the WSLP2010 resistor incorporates a solid metal nickel-chrome or manganese-copper alloy resistive element with low TCR (< 20 PPM/░C). This results in a high-power resistor with an operating temperature range of − 65 ░C to + 170 ░C, while maintaining the superior electrical characteristics of the Power Metal Strip construction.

The new device allows for the design of high-power circuits featuring the smallest possible resistor for higher-performance end products. Furthermore, the resistor’s high-temperature capability allows the use of the WSLP2010 in harsh, high-temperature environments without sacrificing power rating or electrical performance. The WSLP2010 will meet the requirements of AEC-Q200.

The resistor is ideal for all types of current sensing and pulse applications, including switching and linear power supplies, instruments, and power amplifiers in automotive electronic controls such as engine, brushless DC motors, anti-lock brakes, and climate controls; industrial controls, including down-hole test/measurement equipment for oil/gas well drilling; inverter controls for HVAC systems; and DC/DC converters for servers, VRMs for laptops, and Li-Ion battery safety and management.

Like all Power Metal Strip resistors, the device released today features an all-welded construction that contributes to its superior electrical performance. A proprietary processing technique produces extremely low resistance values ranging from 0.001 Ω to 0.01 Ω, with tight tolerances of 0.5 % and 1.0 %.The WSLP2010 provides very low inductance of 0.5 ηH to 5 ηH and low thermal EMF (< 3 ÁV/░C). The device is lead (Pb)-free and RoHS-compliant.

Samples and production quantities of the new resistor are available now, with a lead time of 12 to 16 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology, Inc.