Vishay Intertechnology to Highlight Leading Military-Qualified, DSCC-Approved, and COTS Resistors, MLCCs, and Tantalum Capacitors at CMSE 2013


130212CMSE
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — Feb. 12, 2013 — Vishay Intertechnology, Inc. (NYSE:VSH) today announced that the company will be exhibiting its extensive offering of military-qualified, DSCC-approved, and COTS resistors, high-reliability multilayer ceramic capacitors (MLCC), and tantalum capacitors at the 2013 Components for Military and Space Electronics (CMSE) conference and exhibition. The event will take place Feb. 19-22 at the LAX Radisson Hotel in Los Angeles.

CMSE is the premier conference on designing military and space systems with military-qualified and COTS components, subsystems, and software. At the show, Vishay will be showcasing a wide variety of military-qualified resistors with established reliability. These will include metal, thick, and thin film chip resistors; leaded and housed wirewound devices; and thick and thin film resistor networks.

Vishay’s line of high-reliability MIL-PRF-55681-qualified MLCCs will be on display, in addition to DSCC-approved devices for high-frequency applications. The MLCCs are available in a wide range of body sizes from 0402 to 3640 and with BP, BR, and BX dielectrics. The devices offer a Precious Metal Electrode (PME) internal construction.

Featured military-qualified tantalum capacitors at CMSE 2013 will include through-hole, surface-mount, and high-energy wet tantalum capacitors; hermetically sealed solid tantalum through-hole capacitors with high reliability and low current and dissipation factor; and conformal-coated tantalum chip capacitors. Rounding out Vishay’s offering will be Hi-Rel COTS solid surface-mount tantalum capacitors with MIL screening and voltages to 75 V.

Vishay will also be highlighting high-precision resistors for non-QPL military applications. On display will be ribwound and roundwire resistors with power ratings to 2000 W and resistance down to 0.010 Ω; Power Metal Strip® resistors; metal film resistors with tolerances to ± 0.01 % and flameproof devices with power ratings to 3 W in compact sizes; high- and medium-voltage thick film chips; and high-stability through-hole and surface-mount thin film networks.

For more information on CMSE 2013, please visit http://www.cti-us.com/cmsemain.htm.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

Power Metal Strip is a registered trademark of Vishay Intertechnology.

For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: