Vishay Intertechnology Introduces New Low Input Current Optocouplers in Ultra-Compact SSOP-4 Mini-Flat Package

Devices Offer High CTR From 40 % to 600 % at Low Input Currents of 1 mA


VOS618A VOS617A optocouplers

Products mentioned:

VOS618A
VOS617A
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
MALVERN, Pa. — March 11, 2013 — Vishay Intertechnology, Inc. (VSH: NYSE) is broadening its optoelectronics portfolio with the release of two new series of 4-pin, low- input current optocouplers with phototransistor output. The devices feature low DC input currents of 1 mA (VOS618A) and 5 mA (VOS617A), and are offered in the compact SSOP-4 mini-flat package, which saves more than 60 % board space compared to a DIP-4 package.

VOS618A and VOS617A series optocouplers are designed for isolated feedback loops, I/O isolation, and isolation in switch-mode power supplies, AC adapters, motor drives, solar invertors, networking switches, telecom line cards, and home appliances. The devices protect equipment users from electrical shocks and protect the microprocessors within these systems from being damaged by voltage spikes.

To provide designers with increased flexibility, the half-pitch mini-flat VOS618A and VOS617A series offer a variety of current transfer ratio (CTR) ranges from 40 % to 600 %. The devices, also known as opto-isolators, feature a GaAs infrared emitting diode, which is optically coupled to a silicon planar phototransistor detector. Their SSOP-4 package provides a 3750 VRMS isolation voltage rating, a half lead pitch of 1.27 mm (50 mils), package height of 2 mm, and creepage and clearance distance of ≥ 5 mm.

The new series of optocouplers are molded using an eco-friendly “green” compound, and are compliant to RoHS Directive 2011/65/EU. They are certified to UL, CSA, VDE, FIMKO, and CQC safety standards.

Samples and production quantities of the new optocouplers are available now, with standard lead times of four to six weeks.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.