Vishay Intertechnology to Showcase Leading MLCCs and Surface-Mount and Wire-Bondable Thin Film Products at IMS 2013


International Microwave Symposium (IMS)
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — May 21, 2013 — Vishay Intertechnology, Inc. (NYSE:VSH) today announced that it will be showcasing the company’s latest industry-leading multi-layer ceramic chip capacitors (MLCCs) and surface-mount and wire-bondable thin film products at the 2013 IEEE MTT International Microwave Symposium (IMS), being held from June 2-7 at the Washington State Convention Center in Seattle.

In booth 2303, Vishay Vitramon will introduce a new line of quad high-frequency, high-power MLCCs in 0505 and 1111 cases with high Q > 2000, ultra-low ESR, and voltage ratings from 25 VDC to 1500 VDC. The devices are optimized for a wide range of high-frequency applications, including MRI coils and generators, RF instrumentation, and impedance matching networks. In addition, Vishay Vitramon will highlight its surface-mount, high-frequency MLCCs in the 0402, 0603, and 0805 case sizes, which are ideal for commercial applications such as VoIP networks; cellular base stations; and satellite, WiFi (802.11), and WiMAX (802.16) wireless communication.

At IMS 2013, Vishay Dale will be showcasing its high-frequency thin film chip resistors for low-noise amplifiers and line termination. Vishay Electro-Films (EFI) will be demonstrating surface-mount thin film RF capacitors for lumped element filters and impedance matching circuits, and wire-bondable thin film RF spiral inductors for RF tuning circuits and RF choking for DC biasing. In addition, Vishay EFI’s RF filters and substrates will be on display. They offer a wide selection of materials and packaging capabilities, and are qualified up to 70 GHz.

Part of International Microwave Week, IMS is the world’s premier microwave conference. It features a large trade show, technical sessions, workshops, and panel sessions covering a wide range of topics, including wireless communication, radar, RF technologies, microwave electronics and applications, and more.

For more information on IMS 2013, visit http://www.ims2013.org/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.