Vishay Intertechnology’s New FRED Pt Hyperfast and Ultrafast Recovery Rectifiers Reduce Switching Losses in Consumer Products and Electronic Ballast Lighting

3 A to 5 A Rectifiers in SMA, SMB, and SMC Packages Increase Power Density
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
MALVERN, Pa. — June 6, 2013 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced 10 solderable FRED Pt Hyperfast and Ultrafast recovery rectifiers that include the industry’s first 3 A devices in the SMA package, 3 A and 4 A devices in the SMB package, and 4 A and 5 A devices in the SMC package. Combining extremely fast and soft recovery characteristics with low forward voltage drop and low leakage current, the new rectifiers reduce switching losses in consumer products, LCD TVs, power supplies, and electronic ballast lighting.

The FRED Pt rectifiers released today offer designers a choice of current ratings, packages, and speeds to optimize efficiency in their applications. With forward currents up to 3 A in the SMA package, 4 A in the SMB package, and 5 A in the SMC package, the devices increase power density to facilitate lower system costs. “U Speed” Ultrafast rectifiers offer the advantage of lower forward voltage, while “H Speed” Hyperfast devices provide a lower reverse recovery charge.

The FRED Pt rectifiers are intended for power factor correction (PFC) diodes, boost diodes for discontinuous conduction mode (DCM) and critical conduction mode (CRM), and freewheeling diodes in power switching applications. The devices feature a planar structure and platinum doped lifetime control to guarantee high overall performance, ruggedness, and reliability characteristics. The components offer an operating junction temperature to +175 C for a more robust design.

The devices offer an MSL moisture level of 1 per J-STD-020, LF maximum peak of +260 C, are RoHS-compliant and are halogen-free.

Device Specification Table:

Part # Package IF(AV) (A) VR (V) VF at IF (V) Typ trr at rated IF (ns) Speed
VS-3EGH06-M3 SMB 3 600 1.7 35 Hyperfast − Low Qrr
VS-3EGU06-M3 SMB 3 600 1.35 41 Ultrafast − Low VF
VS-3EMH06-M3 SMA 3 600 1.7 35 Hyperfast − Low Qrr
VS-3EMU06-M3 SMA 3 600 1.35 41 Ultrafast − Low VF
VS-4ECH06-M3 SMC 4 600 1.85 30 Hyperfast − Low Qrr
VS-4ECU06-M3 SMC 4 600 1.3 45 Ultrafast − Low VF
VS-4EGH06-M3 SMB 4 600 1.95 30 Hyperfast − Low Qrr
VS-4EGU06-M3 SMB 4 600 1.3 45 Ultrafast − Low VF
VS-5ECH06-M3 SMC 5 600 1.95 30 Hyperfast − Low Qrr
VS-5ECU06-M3 SMC 5 600 1.35 45 Ultrafast − Low VF

Samples and production quantities of the new FRED Pt rectifiers are available now, with lead times of 12 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

FRED Pt is a registered trademark of Vishay Intertechnology