Vishay Intertechnology’s New Thermal Fuses are Industry’s First to Combine High Currents to 55 A With Operating Temperatures to + 160 C for 1000 Hours


HCTF HCTF 235 fuses

Products mentioned:

HCTF Series
HCTF CP Series
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
MALVERN, Pa. — June 18, 2013 — Vishay Intertechnology, Inc. (NYSE: VSH) today introduced the industry’s first thermal fuses to offer high current capabilities up to 55 A and operation at temperatures up to + 160 C for 1000 hours without unexpected breakdown. AEC-Q200 tested, devices in the new Vishay Beyschlag HCTF series provide a safety interrupt of electrical power in high-current automotive applications.

In the case of excess heat in the range of the functioning temperature of +235 C ( 15 K), HCTF thermal fuses open automatically and disconnect the circuit. Typical applications for HCTF devices include automotive power electronics that can be connected to steady battery power (B+ or terminal number 30), such as control units of fans and pumps for liquid engine cooling, inlet air control units, diesel pre-heaters, engine control units, ABS control units, and diesel heater plugs relays.

The thermal fuses offer significantly higher current capabilities than other devices on the market, which are limited to 25 A at an ambient temperature of 23 C, or 12 A at an ambient temperature of 100 C. The HCTF devices’ robust, solid-state design, in combination with low cold resistance of = 0.1 mΩ, guarantees extended reliability at high current loads and ambient temperatures.

Devices in the HCTF series are RoHS-compliant and offer a rated voltage of 24 V. HCTF 235 fuses can be assembled with electric resistance welding, while HCTF 235 CP devices can be inserted into clamp terminations. In either case, both versions can be assembled with crimping units as well.

Samples and production quantities of the new thermal fuses are available now, with a lead time of 14 weeks for larger orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.