Vishay Intertechnology to Showcase Industry-Leading Innovations Across all Product Lines at Techno-Frontier 2013

Latest Semiconductors and Passive Components Increase Efficiency and Reliability in Wide Range of Applications


Techno-Frontier 2013
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
MALVERN, Pa. — July 3, 2013 — Vishay Intertechnology, Inc. (NYSE:VSH) today announced that it will be exhibiting its latest semiconductors and passive components in booth 1D-207 at Power System Japan, a focused exhibition on power systems at Techno-Frontier 2013, being held at the Tokyo Big Sight from July 17 to 19, 2013. A component solutions provider for connectivity, mobility, and sustainability, Vishay will be highlighting industry-leading innovations across all of its product lines that provide increased efficiency and reliability for a wide range of applications.

At Techno-Frontier 2013, Vishay Siliconix will be showcasing TrenchFET® Gen IV MOSFETs with maximum on-resistance down to 0.00135 ? at a 4.5 V gate drive; 50 W front-lighting LED drivers in PowerPAK® SO-8L and 8x8L packages; and thermally and electrically optimized PowerPAIR® devices. Highlighted power ICs will include 28 V programmable, protected smart load switches in the 3 mm by 3 mm DFN10 package; high-density 60 A power stages in 5 mm by 5 mm packages; and high-efficiency 16 V microBUCK® regulators in 3 mm by 3 mm QFN-16 packages.

Vishay Semiconductors will be featuring a variety of diodes, including 45 V to 120 V TMBS® Trench MOS Barrier Schottky rectifiers in the SMPD package; Gen2 650 V FRED Pt® Ultrafast diodes for electric vehicles, UPS, and solar inverters; and FRED Pt Hyperfast and Ultrafast recovery rectifiers. In addition, Vishay Semiconductors will highlight optoelectronics products such as SurfLight™ high-power infrared surface emitters; fully integrated proximity sensors with digital output; and 1 mA and 5 mA input current optocouplers.

Passive components from Vishay will consist of a wide variety of the company’s latest capacitors, resistors, and inductors. Highlighted resistors will include Vishay Dale Power Metal Strip® resistors with high power density and high-temperature capabilities to +275 °C for harsh environments, in addition to high-current Power Metal Strip shunts for power meter and battery management applications.

Featured capacitors will include Vishay Sprague Micro Tan® automotive-grade solid tantalum chip capacitors in the industry's smallest case sizes; Vishay ESTA power electronics capacitors; and Vishay Vitramon safety-certified multilayer ceramic chip capacitors (MLCCs). Vishay Dale will be showcasing inductors such as low-profile, high-current IHLP® devices for automotive applications, and high-temperature through-hole inductors for desktops and servers.

In addition, Vishay will be offering two demonstrations in its booth at Techno-Frontier 2013. Vishay Siliconix will be demonstrating the increased efficiency provided by its 600 V and 650 V E Series power MOSFETs. Vishay Semiconductors will be providing a system demonstration that highlights the low forward voltage and fast turn-on times of TMBS rectifiers, and high impedance and reduced signal loss of low CJ TVS.

For more information on Techno-Frontier 2013, please visit http://www.jma.or.jp/TF/en/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.

http://twitter.com/vishayindust
http://www.facebook.com/VishayIntertechnology

###

TrenchFET, PowerPAK, PowerPAIR and microBUCK are registered trademarks of Siliconix incorporated. Power Metal Strip, MicroTan and IHLP are registered trademarks of Vishay Intertechnology.