Vishay Intertechnology Claims Six Spots on Electronic Design’s Annual “Top 101 Components"

IWAS-3827EC-50 Wireless Charging Receiving Coil Listed in the Top 10


For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — July 23, 2013 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that the company’s IWAS-3827EC-50 wireless charging receiving coil, VCNL3020 proximity sensor, SMA6F transient voltage suppressors (TVS), P16S panel potentiometer,193 PUR-SI Solar power aluminum capacitors, and VLMU3100 ultraviolet (UV) LED have been selected for Electronic Design’s “Top 101 Components.” The annual list compiles the 101 most popular components from the previous year among readers of the magazine’s Products of the Week newsletter. The complete list is available on the magazine’s website here: http://electronicdesign.com/components/top-101-components-2013

#8 − IWAS-3827EC-50 Wireless Charging Receiving Coil

For the wireless charging of 5 V portable electronics, the powdered-iron-based, WPC-compliant (Wireless Power Consortium) IWAS-3827EC-50 offers a durable construction, high permeability shielding, and high efficiency greater than 70 %. With dimensions of 38 mm by 27 mm, the device is 33 % smaller than the standard 48 mm by 32 mm IWAS-4832FF-50 Rx coil.

Link to product datasheet ( IWAS-3827EC-50)

#21 − VCNL3020 Proximity Sensor

The VCNL3020 is a fully integrated proximity sensor that combines an IR emitter, photo-pin-diode, signal processing IC, and 16-bit ADC in one small 4.85 mm x 2.35 mm x 0.83 mm surface-mount package. The space-saving device supports an easy-to-use I2C bus communication interface, and features an interrupt function and an integrated external emitter driver.

Link to product datasheet (VCNL3020)

#40 − SMA6F TVS

Offered in the SlimSMA™ DO-221AC package, the SMA6F series of TransZorb® TVS features a low profile of 0.95 mm, high surge capability to 600 W at 10/1000 µs and 4 kW at 8/20 µs, and excellent clamping capability. SMA6F TVS are 50 % thinner than devices in the traditional SMA package, yet are footprint compatible and offer 50 % higher surge capability.

Link to product datasheet (SMA6F)

#73 − P16S Panel Potentiometer

The P16S is the industry’s first panel potentiometer to include a variable resistor and switch incorporated into a built-in knob. Featuring a compact, fully sealed, and panel-sealed construction, the device is designed for military, professional audio, and industrial applications that require volume, speed, intensity, and voltage controls in a compact design.

Link to product datasheet (P16S)

#74 − 193 PUR-SI Solar Power Aluminum Capacitors

The 193 PUR-SI Solar series of snap-in power aluminum capacitors offers a rated voltage of 500 V at 50 °C and a category voltage of 450 V at +105 °C. Targeted at solar applications, where the highest voltage is present under no load conditions, the devices also feature a long useful life and rated ripple current up to 2.52 A at +105 °C and 100 Hz.

Link to product datasheet (193 PUR-SI Solar)

#82 − VLMU3100 UV LED

Aimed at a wide range of applications, including adhesive curing, the VLMU3100 UV LED serves as a solid-state replacement for mercury vapor lamps. The device features a typical luminous intensity of 11 mcd at 20 mA, with a typical wavelength of 405 nm and forward voltage of 3.2 V for low power consumption.

Link to product datasheet ( VLMU3100 )

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.