Vishay Intertechnology’s New BiSy Single-Line ESD Protection Diode Saves Board Space in Portable Electronics

Device Features Ultra-Compact CLP0603 Package With Low Profile of 0.27 mm and Low Capacitance of < 0.8 pF


V10PN50 V15PN50 diodes
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
MALVERN, Pa. — Aug. 15, 2013 — Vishay Intertechnology, Inc. (NYSE: VSH) today released a new bidirectional symmetrical (BiSy) single-line ESD protection diode for portable electronics in the ultra-compact CLP0603 package. Measuring only 0.6 mm by 0.3 mm with a very low height of 0.27 mm, the VBUS05A1-SD0 offers low capacitance and leakage current for the protection of high-speed data lines against transient voltage signals.

The VBUS05A1-SD0 uses a 0603 (metric) chip-level package that is one the smallest in the industry, requiring three times less board space than packages with a 1006 (metric) size. Due to its short leads and small package size, the diode’s line inductance is very low, allowing fast transients such as an ESD strike to be clamped with minimal over- or undershoots.

With a very low load capacitance of < 0.8 pF, the VBUS05A1-SD0 can be used for the protection of high-speed data ports like HDMI, USB 3.0, and Thunderbolt in portable gaming systems, digital cameras, MP3 players, and mobile phones. The device features a low maximum leakage current of < 0.1 A at the working voltage of 5.5 V, a breakdown voltage of typical 8.8 V at 1 mA, and a maximum clamping voltage of 18 V at 2.5 A.

The VBUS05A1-SD0 provides transient protection for one data line as per IEC 61000-4-2 at 13 kV (air and contact discharge). The device is lead (Pb)-free, halogen-free, RoHS-compliant, and conforms to Vishay “Green” standards.

Samples of the new VBUS05A1-SD0 are available now. Production quantities will be available in Q4 2013, with lead times of eight weeks for large orders.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.