Vishay Intertechnology to Showcase Leading Vishay Electro-Films Products at 2014 SPIE Photonics West Exhibition


Vishay Intertechnology to Showcase Leading Vishay Electro-Films Products at 2014 SPIE Photonics West Exhibition
For more information:
Media contact -  Bob Decker, Red Pines Group
Phone:  1.415.409.0233 
Fax:  1.650.618.1512 
E-mail:  bob.decker@redpinesgroup.com

Sales contact: 

MALVERN, Pa. — Jan. 28, 2014 — Vishay Intertechnology, Inc. (NYSE: VSH) today announced that it will be showcasing its latest industry-leading Vishay Electro-Films (EFI) solutions at the 2014 SPIE Photonics West Exhibition, taking place from Feb. 4-6 at the Moscone Center in San Francisco. In booth 5618, products on display will include a wide range of Vishay EFI custom submounts, custom substrates with sidewall patterning, high-performance RF capacitors, and wire-bondable products.

At the 2014 SPIE Photonics West Exhibition, featured submounts will include Vishay EFI's AlN (Aluminum Nitride), BeO (Beryllium Oxide), and Al203 (Aluminum Oxide) ceramic substrates, which offer copper-filled vias, thick copper traces, and laser-machined shapes. For bonding, gold/tin solder features 70/30 to 80/20 compositions and thickness from 2 m to 8 m. Also on display will be Vishay EFI's custom substrates with sidewall patterning. Ideal for high-frequency circuits in RF applications and high-bit-rate transceivers, the substrates feature a plate thickness ≤ 0.025 in, minimum gap of 0.003 in, and are available in a variety of metal systems.

For impedance matching circuits, decoupling, DC blocking, and lumped element filters, Vishay EFI will be highlighting its RFCS surface-mount thin film RF capacitors. The devices feature capacitance from 0.2 pF to 27 pF, low DCR, and high Q and SRF. Highlighted wire-bondable products will include resistors with TCR to 25 ppm/C and power ratings to 1 W; resistor networks with tolerances to 0.05 %; single and binary capacitors; and inductors with inductance from 3 nH to 150 nH.

Presented by SPIE − the international society for optics and photonics − the Photonics West Exhibition is the essential photonics and laser event, highlighting the latest products, tools, and applications. For more information on the event, visit http://spie.org/.

Vishay Intertechnology, Inc., a Fortune 1000 Company listed on the NYSE (VSH), is one of the world's largest manufacturers of discrete semiconductors (diodes, MOSFETs, and infrared optoelectronics) and passive electronic components (resistors, inductors, and capacitors). These components are used in virtually all types of electronic devices and equipment, in the industrial, computing, automotive, consumer, telecommunications, military, aerospace, power supplies, and medical markets. Vishay’s product innovations, successful acquisition strategy, and "one-stop shop" service have made it a global industry leader. Vishay can be found on the Internet at www.vishay.com.